Veelgestelde vragen (FAQ's) zoeken
Can TeSys T be connected to Profibus?
Yes, TeSys T motor management modules can communicate with all the most commonly used protocols, including profibus.
The offer is structured as follows:
The offer is structured as follows:
- 3 ratings: 8A, 27A, 100A, resulting in 3 different part numbers: LTMR08***, LTMR27***, LTMR100***
- Two power supply ranges: 24v DC and 110-240v AC, indicated respectively by the letters BD and FM at the end of the part number. For example, LTMR***BD for 24v DC.
- Five possible networks indicated by the letters M (Modbus), C (CANopen), D (DeviceNet), P (Profibus) and E (Ethernet). For example, LTMR**PBD or LTMR**PFM for Profibus
- go to www.se.com
- in the search bar, type "Tesys B12"
- click on the result under "Documentation" that says "Tesys - chapter B12..."
- dowload
Gepubliceerd voor:Schneider Electric Netherlands
Ontdek meer
Productfamilie
Ontdek meer
Productfamilie