Veelgestelde vragen (FAQ's) zoeken
Can the HMI of the Micrologic X unit be replaced?
The embedded Micrologic X display/wireless module is field replaceable.
It allows to secure customer service quality in case of defect: no need to change the complete control unit, then service continuity with basic protection is guaranteed.
Moreover at the same time it allows to be ready for future evolutions on wireless communication for example.
It allows to secure customer service quality in case of defect: no need to change the complete control unit, then service continuity with basic protection is guaranteed.
Moreover at the same time it allows to be ready for future evolutions on wireless communication for example.
Gepubliceerd voor:Schneider Electric Netherlands
Ontdek meer
Productfamilie
Ontdek meer
Productfamilie