Veelgestelde vragen (FAQ's) zoeken
Can a side mount auxiliary contact be fitted to the contactor in an LE1D series DOL starter?
You cannot mount side auxiliaries to the contactors in the LE1D09* & LE1D12* DOL starters because the internal width between the side of the TeSys Deca contactors and the enclosure is approximately 8mm. As the side auxiliaries are 12.5mm wide, there is not enough space to mount the side auxiliaries and ensure correct operation.
However, is it possible on the LE1D18*, LE1D25* and LE1D35* & LE1D40A*, LE1D50A* and LE1D65A* DOL starters, providing you mount the auxiliary block on the right hand side of the contactor.
However, is it possible on the LE1D18*, LE1D25* and LE1D35* & LE1D40A*, LE1D50A* and LE1D65A* DOL starters, providing you mount the auxiliary block on the right hand side of the contactor.
Gepubliceerd voor:Schneider Electric Netherlands
Ontdek meer
Productfamilie
Ontdek meer
Productfamilie