Søk i ofte stilte spørsmål (FAQ)
STB Module Editor Diagnostics Tab Information
Goals and Symptoms
This resolution provides cause and suggested corrective action information about error codes which are displayed in STBSPU1000 Configuration Software using the Module Editor Diagnostics tab.
Causes and Fixes
Reference Attachments for an error table. The read only Diagnostics tab screen is accessible when configuration software is in the online mode. The tab is grayed out when the software is in the offline mode. The screen displays error messages generated by the module selected in the Island Editor and is accessed by double clicking on the module.
Attachments
(Removed File URL: 176073_AF1A/STB_Diagnostics_Tab.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/8d570d63ae5bf865c125728c00161844/fl_block_5/0.1350?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL176073 V2.0, Originally authored by WeDa on 02/24/2007, Last Edited by WeDa on 02/24/2007
Related ranges: Advantys STB