Søk i ofte stilte spørsmål (FAQ)
What is the replacement for the Twido TWDDRA16RT 16-point Discrete Output Expansion Module?
Issue:
What is the replacement for the TWDDRA16RT?
Product line:
Twido, OTB, TWD, TM2
Cause:
Product obsolescence.
Resolution:
The replacement is the Twido TM2DRA16RT 16-point Discrete Output Expansion Module. The Twido is obsolete and has been replaced with the M221 and now the TM2DRA16RT modules are also obsolete and that is now replaces with the TM3DQ16R. This will not work with the Twido's or the OTB"s.
Publisert for:Schneider Electric Norway
Finn ut mer
Rekkevidde:
Finn ut mer
Rekkevidde: