Søk i ofte stilte spørsmål (FAQ)
Is the CM2050 compatible with the IOM (Input/Output Module)?
The CM2050 is compatible with all IOMs models. However, the CM2050 does NOT have onboard alarm/relay functions. Consequently, the CM2050 can NOT internally control a relay output. However, software or a PLC can be used remotely to energize output relays of the IOM. Additionally, the KYZ pulse output and analog input/output features of the various IOMs will function properly with the CM2050.
Legacy KB System (APS) Data: RESL185165 V2.0, Originally authored by KBAdPM on 06/27/2007, Last Edited by MaTh on 10/06/2010
Related ranges: CM2000 series
Publisert for:Schneider Electric Norway
Finn ut mer
Rekkevidde:
Finn ut mer
Rekkevidde: