Søk i ofte stilte spørsmål (FAQ)
Can setpoint modules be configured from the Dashboard view in Power Monitoring Expert (PME) Web Applications?
Issue
Is it possible to configure the setpoint module from the Web Applications Dashboards tab?
Product Line
Struxureware Power Monitoring Expert 7, 8.x, 9, 2020
Environment
Web Applications - Dashboard Tab
Resolution
No. Setpoint modules can only be set up and modified in PME Designer, PME Vista, or ION Setup software.
Publisert for:Schneider Electric Norway
Finn ut mer
Rekkevidde:
Finn ut mer
Rekkevidde: