Søk i ofte stilte spørsmål (FAQ)
Can we deliver the medium power transformers completely without oil?
Yes, this is possible for Medium Power Transformers, however it's recommended to keep the transformer without filling the oil for a maximum of 6 months period. For cases where the transformer will be stored more than 6 months we recommend to dispatch the transformer with oil inside.