Søk i ofte stilte spørsmål (FAQ)
Osisense XC - Datasheet of the adapted XCMD connection component ZCMC21T2SF
Attached the datasheet of adapted XCMD connection component ZCMC21T2SF, using a special cable halogen free for railway equipments, complying to EN 50306 and EN 45545 standards. It can be associated to ZCMD21 body. This reference is available to order without any restriction. It is not in stock, it is produced at order reception by the assembly plant.
Publisert for:Schneider Electric Norway
Vedlegg
Finn ut mer
Kategori:
Rekkevidde:
Produkt:
Finn ut mer
Kategori:
Rekkevidde:
Produkt: