Søk i ofte stilte spørsmål (FAQ)
Is there a meter that supports Class 200 and Class 20 applications?
Produce Line
ION8600, ION8650
EV55
Environment
Meter selection
Resolution
The ION8650 series supports the following meter socket options:
The EV55 series supports the following meter socket options:
ION8600, ION8650
EV55
Environment
Meter selection
Resolution
The ION8650 series supports the following meter socket options:
- Class 1/2/10/20 - 9S, 29S, 36S, and 35S
The EV55 series supports the following meter socket options:
- Class 200 - 2S, 12S, and 16S
- Class 20 - 5S, 6S, and 9S
Publisert for:Schneider Electric Norway
Vedlegg
Finn ut mer
Rekkevidde:
Finn ut mer
Rekkevidde: