Søk i ofte stilte spørsmål (FAQ)
Osisense XC - What is the UL94 flame classification of the black XCKS plastic case?
The thermoplastic case (housing & cover) of the black XCKS limit switch is a LEXAN 500R, or polycarbonate PC GF10. It is flame classified UL94 V-0.
Publisert for:Schneider Electric Norway
Finn ut mer