Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What is the part number for ATV61 and ATV71 Ethernet IP card?
Issue:
ATV61 and ATV71 Ethernet IP card part number

Product Line:
Altivar 61 and Altivar 71 drives, all serial numbers

Environment:
All

Cause:
Need part number for Ethernet IP card

Resolution:
The part number for the Ethernet IP card is VW3A3316. This card has Ethernet IP functionality only.
The VW3A3320 option card has Ethernet IP and Modbus TCP functionality.