Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What is the operation of dynamic braking on Altivar 71 drive with braking resistor.
For dynamic braking with braking resistor, the drive switches on the braking transistor when the value of bus voltage
is more than threshold voltage. If the value of the bus voltage is less at the same threshold, the transistor switch off
Refer to attached file for voltage value: The threshold is OBR.

Schneider Electric Sverige

Bilagor
ATV71_DCbus voltage safety threshold.pdf [7.42 KB]