Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What is the address of the Com Scanner input and Com Scanner output on the ATV61 / ATV71 Series Drives?

Article available in these languages: Spanska

ISSUE:
Needs the register address for the data from the Com Scanner input and Com Scanner output on the ATV61 / ATV71 Series Drives

Product Line:
Altivar 61 / Altivar 71 series drives.

Environment:
All models, All serial numbers.

Cause:
Drive is configured for communication control via the com scanner input and output but the base address of the com scanner input and output is unknown.

Resolution:
The base address of the com scanner input is 12741.
The base address of the com scanner output is 12761.