Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Can the Adapter Plate that is used to replace the ATV58 with the ATV61/71 be used when converting the Flex58 to the ATV61/71?
Issue:
Converting the Flex58 to the ATV61/71 using Adapter plate?

Product Line:
ATV61 and ATV71

Environment:
Frame size 2 to frame size 8

Cause:
Converting from the ATV58/FLEX58 to the ATV61/71

Resolution:
The Adapter plate that is used for mounting the ATV61/ATV71 in the same foot print as the ATV58 cannot be used to replace the FLEX58 with the ATV61/71 . The foot print of the FLEX58 is different from that of the ATV58, this difference is not compatible with the mounting plate.