Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Why can't I create a project offline with my variable frequency drive with SoMove?
Issue:
Creating an Offline Project with SoMove

Product Line:
SoMove

Environment:
Build 2.2 and later

Cause:
The most likely cause is that the DTM files need to be downloaded and installed.

Resolution:
Use this link to download the current version of the Altivar and Altistart DTM files for SOMove.

ATV
https://www.se.com/ww/en/download/document/Altivar_DTM_Library?showAsIframe=true&xtmc=altivar dtm&xtcr=1

ATS
https://www.se.com/ww/en/download/document/Altistart_DTM_Library?showAsIframe=true&xtmc=altistart dtm&xtcr=1

SoMove Standalone V2.2
https://www.se.com/download/ww/en/results/0/0/8336271-SoMove/1555684/?showAsIframe=false