The maximum number of times the power of the Altivar71 that is permitted to be switched is 1 cycle every minute. If the switching cycle is more in a minute the drive filter capacitors get stressed too much.
It is better to command the on/off of the drive by Logic Input.
It is better to command the on/off of the drive by Logic Input.
Publicerad för: Schneider Electric Sverige