Prehľadávať FAQ
Can Modbus RTU be transmitted over a modem connection?
Answer: No, since Modbus RTU is sensitive to inconsistent time delays between characters. A suggested workaround is converting the communications to Modbus ASCII for the modem part of the communications connection. See the attached document for more details.
Originally article#1185