Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Wiring a 2-wire Transmitter to an STBACI0320 Analog Input
Issue
This resolution describes how to wire 2-wire analog transmitters to the inputs of an STBACI0320 analog input module.


Product Line
Advantys STB
STBACI0320


Environment


Resolution
2-wire analog transmitters require a loop power supply to power the loop. The following diagrams describe how this is done with separate power supplies for each loop or a single power supply for all loops.

Wiring diagram for isolated loop power supplies

Wiring diagram for multiple loops using a single source power supply.