Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Can a high potential dielectric test be performed on the ATS22 or ATS48 soft starter?
Issue:
High potential dielectric test.

Product Line:
ATS22, ATS48

Environment:
All models and serial numbers

Cause:
None

Resolution:
No.  Do not perform high potential dielectric (hi-pot) tests on the soft starter or to circuits connected to the soft starter.  Doing so will risk damage to the soft starter.