Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Opening a Unity pro (Version less than 10) project with LL984 library in Unity pro 10
Issue

Opening a Unity pro STA application built with LL984 library in Unity pro 10, generates these kinds of warnings:

LL_SENS_I    Type not found in Types Library,
LL_UCTR    Type not found in Types Library,
LL_T01    Type not found in Types Library,
LL_T001    Type not found in Types Library



Product Line

Unity

Resolution

- install the LL984 library with the according Unity version
- open the unity STA file in Unity 10
- export the XEF or ZEF
- import the XEF or ZEF
- build the project.