Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
What is fault reset on the ATV61/71?
Issue:
Fault reset on ATV61/71

Product Line:
Altivar 61, Altivar 71

Environment:
All serial numbers

Cause:
N/A

Resolution:
Fault reset is a parameter that can be assigned to a logic input that will reset any resettable fault after the fault has cleared.

See attachment


Schneider Electric Slovakia

Príloha(-y)
Fault reset.png [480.62 KB]