Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Video: How do I program my ATV312 drive to run in reverse via logic input?
Issue:
Program my ATV312 drive to run in reverse via logic input

Product Line:
ATV312 series drives.

Environment:
All models, All serial numbers.

Cause:
Unable to find directions in existing literature.

Resolution:
The rrS parameter, under the I-O menu is used to assign "run reverse" to a logic input.  By default, this is assigned to LI2 if the drive is in 2 wire control, and LI3 if the drive is in 3 wire control.