Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Example on configuring an NOR to get a timestamp with a DNP3 point
Issue
Provide an example on how to configure a DNP3 point in the BMXNOR0200 to get a timestamp when the point
DNP3 value changes.

Product Line
BMXNOR0200

Environment
Windows 10

Resolution
The following steps can be used to configure the BMXNOR0200 for accessing a DNP3 point with a timestamp
from a SCADA.
  • Click on 'Data Mapping' in the 'Setup' menu list to open the 'Data Mapping' web page.
dF

  • Click on the down arrow next to the textbox labeled 'Select a type id'
ATQRWH

  • Select the DNP3 point type from the drop down list.
RQET
  • Click on Add
ERQT

  • Enter the appropriate information to define the DNP3 point.
  • Select 'CPU Reg Mapping' as 'Value only'.
  • Select 'Default Static Variation' as 'g1v1 Binary In'.
  • Select 'Default Event Variation' as 'g2v2 Binary Input with time'.
  • Click on 'Change'.
RET

  • Click on 'Events' in the 'Setup' menu list.
  • Click on the down arrow next to the textbox labeled 'Select a type id'
ERT

  • Select the event type from the drop down list.
  • Click on 'Add'.
ERT

  • Click on the down arrow next to 'Event Store Mode' and select the appropriate store mode.
  • Click on the down arrow next to 'Buffer String' and select the appropriate buffer string type..
  • Enter the CPU register address that will be used to store the events count.
  • Click on 'Add'.
3T

  • Click on 'Reset Communications' to allow the changes to take effect..
RT

Schneider Electric Slovakia

Objavte viac
Produkt:
Rad:
Objavte viac
Produkt: