Ako vám dnes môžeme pomôcť?

How many MSA141 module can be connected to Sepam 80?

Issue

The user would like to connect multiple MSA141 analog output modules to a Sepam 80 relay and needs to know how many are supported.

Product

Sepam 20 Series
Sepam 40 Series
Sepam 80 Series

Environment

SEPAM protection relays and associated MSA141 analog output modules.

Cause

The user is unsure of module compatibility limitations and the maximum number of MSA141 modules that can be connected to a single Sepam base unit.

Resolution

A Sepam base unit supports only one (1) MSA141 analog output module. Multiple MSA141 modules cannot be installed or used simultaneously with a single Sepam 80 (or Sepam 20/40) base unit.