Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
UP11_Whether it is possible to export M580 config to excel
Question:
Whether it is possible to export M580 config to excel?

Answer:
M580 hardware config supports exporting  through Unity 11.1.
Actually, xhw is an specified xml format. Change the suffix as xml & you could open it by excel & doing further edit.
However, due to its complicated structure (not the xml with standard format), its hard to perform the export from excel.

The alternative solution is directly open the xhw file by advanced text editor(for ins. notepad++), it will facilitate the follow up edit & save which could be imported back into unity.