Prehľadávať FAQ
Osisense XC - XCKM210 or XCKM210H29 limit switch cross-reference
The XCKM210 or XCKM210H29 limit switch has been completely discontinued in November 2003 (obsolete contact version). It was in fact an XCKM102(H29) switch with some contact state indicator; see attached picture. It used the ZCKM2(H29) special contact body. It is replaced by the XCKM110 or XCKM110H29 since 2004, having a new contact block equivalent to the previous one
Publikované pre:Schneider Electric Slovakia
Príloha(-y)
Objavte viac
Objavte viac