Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
How to show a record for each alarm state change in Vijeo Designer?
Issue:
Looking for a way for the HMI to record a separate entry in the Alarm Summary whenever the alarm transitions from Active, ACK'd, and return to normal.

Product Line:
Vijeo Designer (all versions)

Resolution:
In Vijeo Designer, it is possible to show a separate record in the Alarm Summary for each state change of an Alarm Variable. To do so, simply set the property "Alarm & Events List" to Log.

By default, this property is set to "Active". In this mode, the Alarm Summary will only show alarms that are still Active. When the states change from Active to RTN, the record disappears.