Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Video: How to create an application displayed in popup with Ecostruxure Machine Scada Expert
ow to create an application displayed like a popup with Ecostruxure Machine Scada Expert (VijeoXL)

In the menu Project / Viewer, unselect the option 'Start Maximum'
Possibity to select the option "menu" or and "Rezise Border"

In the tab "Graphics" of "Project explorer", double click on "Graphic script"
Then add the following command in the Sub Graphic_OnStart()

$SetViewerPos (pos x, pos y, size x, size y)

See video for more details
https://www.youtube.com/watch?v=Ld8iBNJ-DH0​