Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
What is the purpose of firmware upgrade in energy meter ?

Issue
What is the purpose of a firmware upgrade in an energy meter?


Product line
PowerLogic™ Energy Meters (including PM series such as PM2225)

Environment
Energy metering systems where performance optimization, feature enhancements, or compliance updates are required

Resolution

There are several reasons to upgrade your meter’s firmware:

  • Improve meter performance (e.g. optimize processing speed)
  • Enhance existing features and functions
  • Add new functionality to the meter
  • Ensure compliance with new or updated industry standards