Prehľadávať FAQ
What is SCADAPack Configurator (Standard) for SCADAPack Workbench?
Issue
Why do I need SCADAPack Configurator for SCADAPack Standard? Previously I was only using ISaGRAF 3.55 to program my SCADAPack.
Product Line
SCADAPack Standard RTU Line
Environment
ISaGRAF 3.55, SCADAPack Workbench
Resolution
Previously in ISaGRAF 3.55, the end user would need to write the SCADAPack controller settings (serial port, DNP3, RTC, etc...) by using the Write to Controller command via the Tools > Controller drop down menu. Specific SCADAPack Standard functionality (advanced telemetry functions) is not built into the new Workbench as it was in 3.55. Instead a separate software package called SCADAPack Configurator is needed to perform these operations. Along with being able to read and write all the specific SCADAPack Standard specific settings, SCADAPack Configurator can be used to obtain Watchdog logs, logs obtained from the dlogfcfg & dlogf functions, DNP Master and Slave diagnostics, C/C++ program Loader as well as SCADAPack Security.