Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Can I purchase SCR(s) for an ATS22?

Article available in these languages: španielčina

Issue:
Can I purchase SCR(s) for an ATS22?

Product Line:
ATS22 Altistart Softstart

Environment:
All

Cause:
Inoperative

Resolution:
A part number is available, however, it is not sold in the USA.  Contact Customer Service at Schneider Electric's Repair Depot at 800-950-9550, or replace.  Standard warranty is 18 months.