Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
How to setup Initial values for PLC Tags from HMI
Issue:
Looking for a way to initialize PLC variables with values from the HMI.

Product Line:
Vijeo Designer (all versions)

Resolution:
To set an initial value for your PLC tag, you could define an On Startup action from your HMI to set the values.

The action should use the Word-set Operation as shown in the screen shot below.

CONFIG