Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
What are possible reason for having custom logic faults on TeSysT that has not been detected by SoMove compiler?
SoMove software with TeSysT DTM is not able to simulate complete TeSysT behavior. It can detect syntax errors, but writing a wrong value to an LTMR register is not implemented in a custom logic compiler. For example, if the new TEsysT few version allows a wider range for certain TEsysT parameters, the extended range can be easily implemented into DTM evolution (new DTM version) and so the configuration seen in SOmove will be consistent with TEsysT parameters. But the custom logic compiler is an extra package and does not often pass evolution (The last evolution was done together with TEsysT fw 2.5 when CALL_EOM instruction was implemented).

Based on experience, 99% of errors where the compiler says OK but TEsysT shows custom logic fault is caused by:
- missing "TMP" or "NV" text in the instruction
- wrong value (out of range) is written into LTMR register.
The rest of the errors shown are detected by SOmove compiler.