Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
What does the 7 indicate before the coil voltage code on the LC1K****7** or LP1K****7** contactors?
Issue:
Suffix number 7 on tesys K contactors

Product Line:
Contactors and Overload Relays

Environment:
TeSys K Miniature Contactors and Overload Relays

Resolution:
The 7 indicates slip-on terminal connections instead of the standard screw clamp