Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
How do you set the two wire type to level control on the ATV600 Process drives?
Issue:
Two wire type to level control on the ATV600 Process drives.

Product Line:
ATV630 and ATV930 Process drives

Environment:
All

Cause:
Set two wire type to level to start on power up with start command

Resolution:
Programming example to set up 2 wire for level control.
Main Menu
Complete Settings
Command and References menu
Set 2-Wire type setting to LEL or Level
Done

ATV600 programming manual
https://www.se.com/ww/en/download/document/EAV64318/

Schneider Electric Slovakia

Objavte viac
Produkt:
Objavte viac
Produkt: