Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
How to know a duplicated IP address on BMENUA0100?
Issue
Customer wants to know how to determine if there is an IP address duplicated on the backplane port or on the control port of the BMENUA0100 module.

Product Line
BMENUA0100

Environment
Firmware 1.01.50

Resolution
The following corrections will be taken in consideration in the next release of the BMENUA0100 documentation.