What should I check for if I have no display on an Altivar drive?
Issue:
Troubleshooting steps if there is no display on an Altivar drive.
Product Line:
Altivar Drives
Environment:
All serial numbers for Altivar Drives
Cause:
N/A
Resolution:
Perform this basic steps:
Check line voltage by measuring L1, L2, L3 on the drive itself
Check DC Bus by measuring PA to PC and PO to PC (most drives)
Reseat terminal card (ATV61/71 only)
Remove cable from Modbus port if present
Check +24 to COM and +10 to COM (DC voltage only)
發佈於: 施耐德電機Taiwan