The material composition used in the Main Bus Bar of the Masterpact Air Circuit breaker (ACB) is shown in the table attached.
Note:
AL/Sn5 means Aluminum connector with Sn5 coated
Опубліковано для:Schneider Electric Україна


{}
The material composition used in the Main Bus Bar of the Masterpact Air Circuit breaker (ACB) is shown in the table attached.