Issue:
In order to ensure proper operation, SmartSlot cards must be installed in a certain, specific order according to precedence
Product Line:
Single Phase Symmetra and smart-slot accessories.
Note: Only SmartSlot accessories with revision K or later can be integrated with the Symmetra.
Resolution:
When placing multiple SmartSlot accessories in the Symmetra expansion slots, great care must be taken so the correct ordering of the accessories observed. A SmartSlot device with higher priority must be placed in the SmartSlot labeled with the higher number. Refer to the following table for details.
PART NUMBER | PRIORITY | POSITION | |
---|---|---|---|
Network Management Card | AP9606 | Highest | Highest-numbered slot |
Call-UPS II Out of Band Management SmartSlot Card | AP9608 | Second highest | Second-highest-numbered slot (highest if no network management card is present) |
Dry Contact I/O SmartSlot Card | AP9610 AP9613 | Medium | Any slot numbered lower than a network management card, Call-UPS II; any slot higher than Measure-UPS |
Interface Expander SmartSlot Card | AP9607 | Medium | Any slot numbered lower than a network management card, Call-UPS II; any slot higher than Measure-UPS |
Measure-UPS SmartSlot Card | AP9612T AP9612TH | Lowest | Lowest-numbered slot |
The following graphic is an example of how to install multiple SmartSlot devices in the Symmetra Power Array. Please note the numbering shown in the figure. The network management card is installed in slot #4, Call-UPS II in #3, Interface Expander in #2, and Measure- UPS in #1.
The following graphic is an example of how to install multiple SmartSlot devices in the Symmetra RM and Symmetra LX. The network management card is installed in slot #2 and Call-UPS II is installed in slot #1.
Опубліковано для:Schneider Electric Україна