Issue:
Is ATV212 capable of single phase input?
Product Line:
Altivar ATV212
Environment:
All serial numbers
Cause:
Some drives can be used with single phase supply voltage for three phase motors.
Resolution:
No, the Altivar 212 can only be used with three phase supply voltage to run three phase motors.
Опубліковано для:Schneider Electric Україна