Issue
Do the XBTG Magelis terminals come with a Compact Flash card?
Product Line
Magelis Terminals
Environment
XBTG
Resolution
No, the XBTG terminals do not come with a Compact Flash card. The cards will have to be purchased separately. Any Compact Flash card can be used.
Опубліковано для: Schneider Electric Україна