Issue
What is the part number for the programming cable for the TSX07 Nano PLC?
Product Line
Modicon Nano PLC
Environment
TSXPCX1031
Resolution
The part number for the serial programming cable for the TSX07 Nano PLC is TSXPCX1031. The TSXPCX3030 USB programming cable can alternatively be used but only if the user is using version 4.0 of PL7-07 under WIN2000 Professional.
Опубліковано для: Schneider Electric Україна