issue
The solution interval for the PCFL( KPID) function block is incorrectly defined as a 'Floating Point' radix instead of the expected 'Long (32 Bit) Integer'.
Product Line
ProWORX 32, Concept
Environment
Windows 7
Resolution
Attempts to enter a floating point value will cause the block to return an error.
Download the attached 'PCFL.ZIP' file and extract the PCFL.UCS file to your ..\ProWORX\32\Scripts folder and replace the existing file with it.
Attachments
Опубліковано для: Schneider Electric Україна