Is it possible to associate the energies to the analog output of IOX extender module ?
Issue
End user would like to know if it is possible to associate the energies to the analog output of IOX extender module.
Product
PM8000 Series
Environment
Power Meter
PM8000 Series
Cause
Is it possible to associate the energies to the analog output of IOX extender module?
Resolution
Yes, the 3 energies (real, reactive and apparent) could be associated with analog output of IOX extender.
Опубліковано для: Schneider Electric Україна