Issue
When selecting RS232 in the serial settings of EGX it does not specify 2-wire.
Product Line
EGX100, EGX150, EGX200, EGX300, EGX400
Environment
EGX Serial Communication
Resolution
The RS232 port is by default a 2-wire communication, and the EGX takes this in to consideration automatically.
Опубліковано для: Schneider Electric Україна