Issue
Maximum inrush current for the Enercept Meter
Product Line
Enercept Meter
Environment
Technical Specifications
Resolution
The maximum inrush current is eight times the CT rating
Example: A 200 amp Enercept Meter would have a 1600 amp inrush rating
Опубліковано для:Schneider Electric Україна