Пошук серед найпопулярніших питань
Where can I find the part number for the replacement inlet vent filter for the M-Flex drives?
Issue:
Replacement part number for the inlet vent filter on M-Flex drives.
Product Line:
M-Flex Enclosed drives
Environment:
Only M-Flex
Cause:
Replacement inlet vent Filter assembly
Resolution:
100HP-200HP CT and 125HP- 250HP VT
80444-132-02- output filter bracket qty 1
80444-133-02- inner filter bracket qty 1
80444-134-01- foam filter element qty 1
250HP- 450HP CT and 300HP-500VT
8044-205-01- Filter qty 1
Reference the M-Flex install manual documents 30072-454-07
We no longer provide this part number. You may contact Carolina Gasket and Rubber CO in GREENSBORO N.C. Phone number is 336-217-2821. You may also check any hardware store and just look for 30 pores per inch.