PME 7.2 - When using IE10 and attempting to log in to the Web Applications, an error message shows 'The application needs to restart'
Issue
When logging into the PME 7.2 Web Applications and using a particular version of Internet Explorer 10, it is possible that an error dialog will be displayed stating "An error occurred communicating with the server while loading data. The application needs to restart."



Product Line
Power Monitoring Expert 7.2

Environment
Web Applications

Cause
The browser definition files need to be updated so ASP.NET can recognize Internet Explorer version 10.

Resolution

Install the hotfix that can be downloaded from http://support.microsoft.com/kb/2600088. The hotfix will solve the problem and make all IE10 update versions work fine with PME 7.2.

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: