Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Latest Firmware version of Com'X 200/210 and Natively supported device type in the Energy Server Com'X 200/210
Product Line
COM'X200 / EBX200
COM'X210 / EBX210
Environment
Ethernet Gateway supported devices
Resolution
The latest version of firmware for Com'X 200 is 3.5.54 and the Com'X 210 is 6.8.7.
They can be downloaded from the following links:
COM'X200 firmware
COM'X210 firmware
In addition, review the attached device list for the Natively Supported Device Types.

For instructions on how to upgrade the firmware, view article FA270261.

Schneider Electric Україна

Вкладення
EnergyServers_MasterDeviceListV6_6_5.pdf [399.6 KB]